Skip to main content

Quick Start Guide

In this Quick Start guide we'll cover how to connect the Thing Plus - ESP32-C5 to a computer and then run one of the included MicroPython examples to demonstrate how to set the ESP32-C5 up as a 5GHz WiFi access point and scans for WiFi networks and devices in range. This guide assumes users have a working knowledge of MicroPython and MicroPython interpreters.

Basic Assembly​

Basic assembly for this example just requires plugging the Thing Plus - ESP32-C5 into a computer over USB-C.

The Thing Plus - ESP32-C5 connected over USB-C

The Thing Plus - ESP32-C5 connected over USB-C

MicroPython Example - WiFi Scan​

The Thing Plus - ESP32-C5 comes flashed with MicroPython firmware that includes two simple examples to get started with the ESP32-C5 and wireless networks.

  • Open your preferred MicroPython environment or IDE and connect to the Thing Plus's USB port.
  • Open the "wifi_demo.py" example from the device.
  • Run the example.
  • The Thing Plus - ESP32-C5 creates a WiFi access point, creates a WiFi station and then performs a WiFi access point scan to detect WiFi networks and devices in its range. Once it finishes the scan it prints out all networks and devices it sees over serial:

Screenshot of WiFi scan results

Screenshot of the serial print from the WiFi Demo.

This list includes the WiFi Band, Channel and SSID of all networks and devices it detects in range.